SLAA450G April 2010 – April 2020
For the BSL project, the following modifications needs to be made to the file:
| CCS | IAR |
|---|---|
|
If the linker command file resides in the project path (which is the default), no action is required. |
Project → Options → Linker → Config Override default linker configuration file with the just created file. $PROJ_DIR$ can be used if the xcl file is stored in the same location than the asm file: $PROJ_DIR$\lnk430g2211_bsl.xcl. Otherwise, a full path can be provided to point to the file. |