SLAAEC6A October 2023 – January 2024
The I2C Monitor tab allows users to load existing device configuration files or direct I2C transactions to the device registers. To access this window panel, click on the I2C Monitor button at the bottom of the GUI. The I2C monitor window opens as shown in the figure below. The LOG screen allows users to log or record any I2C transaction. This is useful when users wanted to record device register to use at later time, users can click on the green LED button once and the button turns to red for recording. To stop recording, just click the red LED button once and the button turns back to green.
To load an existing file or to manually write or read I2C transaction, click on the I/O button to open the input/output window.
Figure 3-32 I2C Monitor Window
Figure 3-33 I2C Monitor I/O Window