SLAAEC6A October 2023 – January 2024
Some TAx5x1x devices support several mixing feature, settings are available in this tab. The ADC tab provides the mixing level/coefficient for each of the 4 ADC Mixers as well as the ADC Loopback. The level is in ratio, for example 0.5 represents half of the mixer full-scale range.
Figure 3-26 Mixer ADC TabIn DAC tab, there are eight possible channels from main ASI and two possible channels from Auxiliary channels. The level is ratio of the mixer full-scale and user can enter in the cell provided. Besides the external inputs, there are beep and chirp generators that user can mix in DAC mixer as well.
Figure 3-27 Mixer DAC Tab