SLAAEO8A October 2024 – November 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105
Figure 4-1 ADC Clock Sysconfig Configuration
Figure 4-2 ADC Sampling Mode Sysconfig Configuration
Figure 4-3 ADC Conversion Memory Sysconfig ConfigurationSampling Timer Source: Select the timer used for sampling time counting in automatic sampling mode
CPU poll
For the device listed below, busy will be set after 14 ULPCLK cycles after ADC start conversion bit is set in CTL1 register. This 14 ULPCLK need to take CPU delay to wait for busy bit set, then CPU can poll the busy bit to wait for busy bit clear. Recommend to use MEMx result loading register to poll the ADC conversion done status.
MSPM0C110x, L1x0x, L111x, L134x, Lx22x, Gx10x, Gx50x, Gx51x, H321x.