SLAU640B April 2019 – March 2023
The Low Level View tab, illustrated in #SLAU701305, allows configuration of the devices at the bit-field level. At any time, the controls in Table 4-2 can be used to configure or read from the device.
| Control | Description |
|---|---|
| Register map summary | Displays the devices on the EVM, registers for those devices, and the states of the registers
|
| Write register button | Write to the register highlighted in the register map summary with the value in the Write Data field |
| Write all button | Update all registers shown in the register map summary with the values shown in the Register Map summary |
| Read register button | Read from the register highlighted in the Register Map summary and display the results in the Read Data field Can be used to re-synchronize the GUI with the state of the hardware |
| Read-all button | Read from all registers in the Register Map summary and display the current state of the hardware |
| Load Configuration button | Load a configuration file from disk and register address/data values in the file |
| Save Configuration button | Save a configuration file to disk that contains the current state of the configuration registers |
| Register Data cluster | Manipulate individual accessible bits of the register highlighted in the register map summary |
| Individual register cluster with read or write register buttons | Perform a generic read or write command to the device shown in the Block drop-down box using the address and write data information |
Figure 4-1 Low-Level Register Control Tab