SLAU640B April 2019 – March 2023
Changing the number of frames per multi-frame output by the JESD204 transmitter (ADC device) is configured using the K parameter on the JESD204C tab in the Configuration GUI. This parameter must be matched by the receiving device, and the SYSREF frequency must also be programmed to a compatible frequency. Ensure that the K value complies with the K Min and Step values for the selected JMODE. Refer to the ADC12DJ5200RF/SE operating modes table in the data sheet.