SLAU855A June 2021 – March 2022 TLV320AIC3101 , TLV320AIC3104 , TLV320AIC3104-Q1 , TLV320AIC3105 , TLV320AIC3106 , TLV320AIC3106-Q1 , TLV320AIC3107 , TLV320AIC3109-Q1 , TLV320AIC34
Figure 1-1 AIC310x Control Software SetupLabVIEW® runtime engine, USB-MODEVM drivers and AC-MODEVM drivers will also be installed.
Figure 1-2 Ready to InstallIf this is the first time installing NI LabView package, GUI will install the Package Manager and the run time engines or no operation is needed if it finds the relevant NI packages. Accept the license agreement and hit next to proceed with the installation.
Figure 1-3 NI Package Manager Installation. Next it will install the NI Run Time Engine. Accept the license agreement and hit next to proceed with the installation.
Figure 1-4 Ni Run Time Engine Installation. When installation is complete close the screen by clicking the 'X' and do not reboot the system untill all driver installations are complete.
Figure 1-5 Reboot Screen, hit 'X' to close - do not reboot now. Next it will install the NI VISA Run Time Engine. Click "Deselect All" before hitting the next button, accept the license agreement and hit next to proceed with the installation.
Figure 1-6 Ni Visa Installation.
Figure 1-7 Deselect All for NI
VISA Run Time Engine. During NI run time installation steps, a NI Update Service screen might appear as shown click Yes to proceed. Click 'X' to close the "Reboot Now" screen, do not reboot the system now.
Figure 1-8 NI Update
Service. If NI package was installed previously a "No operation to be performed." screen will appear. Close the screen by clicking the 'X' and proceed with the GUI installation.
Figure 1-9 No Operation
Screen.
Figure 1-11 Setup FinishedThe installation process is now complete for the TLV320AIC310x control software and the required drivers. Prior to connecting the EVM, reboot the PC.