SLAZ742E July 2023 – December 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
DMA Module
Functional
DMA or CPU may lose operation when simultaneously accessing peripheral register across clock resource
DMA and CPU are sourced from MCLK. When MCLK is running at a higher frequency than ULPCLK, DMA or CPU may lose operation when simultaneously accessing the peripheral register sourced from ULPCLK, which include all PD0 peripherals. The accessed peripheral or register does not have to be the same. Note: ADC is a PD0 peripheral, while DMA or CPU accessing SVT_MEMRES or SVT_FIFODATA of ADC has no restriction. Example: Assume that DMA access UART0 register, for example DMA write data to TXDATA, if CPU also access PD0 peripheral during DMA operation, for example CPU read data from TIMG0 CTR, then DMA or CPU may lose the data.
CPU and DMA should not be accessing PD0 peripherals at the same time when MCLK is running at a higher frequency than ULPCLK.