SLAZ742E July 2023 – December 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
UART Module
Functional
BUSY bit setting is delayed for UART IrDA mode
In IrDA mode, the UART.STAT.BUSY bit is set on the second edge of the IrDA start pulse; which means a whole bit transmission would complete before the BUSY status is properly set. During this time if the software polls the BUSY bit, an incorrect indication of UART not being busy would be observed even when the IrDA start pulse is ongoing. BUSY status will be influenced by the baud rate of the UART, the slower the UART transmission the longer time before BUSY is properly set.
Delay for the length of a bit transmission before checking the BUSY status. Alternatively, checking for UART.STAT.BUSY == 0x0, then UART.STAT.BUSY == 0x1, is another workaround to make a dynamic delay independent of baud rate or other ISRs.