SLLA685 July 2026 TCAN4550-Q1 , TCAN4551-Q1
In some cases, the crystal manufacturer has matched the crystal and load capacitance CLoad in a way that cannot be changed, and the actual OSC2 valley voltage is already close to the threshold, posing a risk of mode switching. Figure 3-7 below shows the OSC2 waveform using the ABM11AIG-40.000MHZ-4-1Z-T (4pF, 60Ω) crystal, with a valley voltage of approximately 168mV, which is close to the 150mV detection threshold.
Figure 3-7 OSC2 Waveform (Close to 150mV Threshold, at Risk)To avoid clock mode switching, it is recommended to add a damping resistor Rd in series between the OSC1 pin and the crystal, as shown in Figure 3-8 below. OSC1 is the output pin in crystal clock mode; the bias current flows out of the OSC1 pin to the crystal to initiate and sustain oscillation. Adding Rd limits the current and reduces the drive level DL, thereby reducing the oscillation amplitude. Note: DL = Irms² × RLoad. Increasing CLoad reduces RLoad and thereby reduces DL; when CLoad cannot be changed, reducing Irms also reduces DL.
Figure 3-8 OSC1 Damping Resistor RdFigure 3-9 below shows the OSC2 waveform after adding a 100Ω Rd. Compared to Figure 3-7, the minimum voltage improves from 168mV to 424mV, a significant improvement that provides ample margin to avoid clock mode switching.
Figure 3-9 OSC2 Waveform (After Adding 100Ω Rd, Significantly Improved)