SLLSEL7B October 2014 – April 2024 DRV8848
PRODUCTION DATA
Bulk capacitance sizing is an important factor in motor drive system design. Bulk capacitance sizing depends on a variety of factors including:
The inductance between the power supply and motor drive system limits the rate that current can change from the power supply. If the local bulk capacitance is too small, the system responds to excessive current demands or dumps from the motor with a change in voltage. Size the bulk capacitance to meet acceptable voltage ripple levels.
The data sheet provides a recommended minimum value, but system-level testing is required to determine the appropriate-sized bulk capacitor.
Figure 7-4 Setup of Motor Drive System With External Power Supply