SLLSFX4A February 2025 – February 2025 TCAN857-Q1
PRODUCTION DATA
The device has several protection features that limit the short-circuit current when a CAN bus line is shorted. The features include CAN driver current limiting in the dominant and recessive states and TXD dominant state timeout which prevents permanently having the higher short-circuit current of a dominant state due to a system fault. During CAN communication the bus switches between the dominant and recessive states; thus, the short-circuit current may be viewed as either the current during each bus state or as a DC average current. When selecting termination resistors or a common mode choke for the CAN design, the average power rating, IOS(AVG), is used. The percentage dominant is limited by the TXD DTO and the CAN protocol which has forced state changes and recessive bits due to bit stuffing, control fields, and interframe space. Making sure there is a minimum amount of recessive time on the bus even if the data field contains a high percentage of dominant bits.
The average short-circuit current of the bus depends on the ratio of recessive to dominant bits and their respective short-circuit currents. The average short-circuit current may be calculated using 2.
Where:
This short-circuit current and the possible fault cases of the network is taken into consideration when sizing the power supply used to generate the transceivers VCC supply.