SLOA338 March 2025 TSD5402-Q1
The purpose of this experiment is to verify how much switching noise the switch-mode power stage introduces to the output of the excitation amplifier. Figure 5-14 shows the test setup circuit diagram for the output spectrum measurement. Similarly, to the transfer function measurement the arbitrary waveform generator is isolated from the input using the isolation transformer. This allows connecting the spectrum analyzer across the amplifier output. A passive 1:10 probe protects the spectrum analyzer input from overload.
Figure 5-15 shows the output spectrum from 0 to 10MHz and selected zoom window from 0 to 1MHz.
Further detailed analysis in Figure 5-16 shows first 8 harmonics. The first unwanted harmonic at 30kHz has 40dB (100x) lower amplitude to the carrier. This is a very good result.
Figure 5-17 shows comparison of the output spectrum when the signal generator drives the input with the harmonic signal (A) and modulated PWM (B). The PWM signal introduces new harmonics.
Figure 5-18 shows detailed analysis of the output signal with the PWM signal as an input. The detail also shows aliased harmonics wrapped around 400kHz. Note that the switching frequency of the TSD5402-Q1 device is 400kHz. However, due to the BD modulation scheme the frequency practically doubles and increase the Nyquist criterion to 400kHz.