SLUAB06 January 2025 AMC131M02 , AMC3330 , ISO7731
In AC injection method, the insulation resistance of the system is obtained by injecting a low voltage AC signal between the positive and negative terminals of the power battery at a certain frequency. The disadvantage is that the test signal creates ripple interference in the system, which affects the normal operation of the system. AC Injection need high accuracy AD/DA, injection capacitor, current sense. RMS detection, low pass, band pass, analyze detected signal… this can be done in dozens milliseconds. Due to the uncertainty about the accuracy, it does not need to be analyzed in this article.