SLUSDU8G September 2019 – January 2025 TPS62860 , TPS62861
PRODUCTION DATA
The TPS6286x has two options to select the output voltage.
The voltage on the VSEL pin can change the output voltage. Putting this pin HIGH selects the output voltage according to VOUT register 2. Putting this pin LOW selects the voltage according to VOUT Register 1. The pin can be toggled during operation.
The pin can also be selected by the value in the VOUT register that is chosen by VSEL at the moment. The voltage changes right after the I2C command is received.