SLUSFU6A September 2025 – November 2025 UCC27834-Q1 , UCC27884-Q1
PRODUCTION DATA
The UCC278X4-Q1 device output stage features a unique architecture on the pull up structure which delivers the highest peak-source current when the time when the power switch is turning on is most needed during the Miller plateau region of the power-switch turn on transition (when the power switch drain or collector voltage experiences dV/dt). The output stage pull-up structure features a P-Channel MOSFET and an additional N-Channel MOSFET in parallel. The function of the N-Channel MOSFET is to provide a brief boost in the peak sourcing current enabling fast turn on. This is accomplished by briefly turning-on the N-Channel MOSFET during a narrow instant when the output is changing state from low to high.
The ROH parameter (see Figure 5-12) is a DC measurement and is representative of the on-resistance of the P-Channel device only. This is because the N-Channel device is held in the off state in DC condition and is turned on only for a narrow instant when output changes state from low to high.
The effective resistance of the UCC278X4-Q1 pull-up stage during the turn-on instant is much lower than what is represented by ROH parameter.
The pull-down structure in the UCC278X4-Q1 is simply composed of a N-Channel MOSFET. The ROL parameter (see Figure 5-13), which is also a DC measurement, is representative of the impedance of the pull-down stage in the device.
Each output stage in the UCC278X4-Q1 is capable of supplying 3.5A peak source and 4A peak sink current pulses. The output voltage swings between (VDD and VSS) and (HB and HS) providing rail-to-rail operation.