The following warnings and cautions are noted for
the safety of anyone using or working close to the TPSM846C26EVM-2PH. Observe all safety precautions.
 | Caution | Hot surface. Contact can cause burns. Do not
touch! TPSM846C26EVM-2PH circuit module
can become hot during operation due to dissipation of heat. Avoid
contact with the board. Follow all applicable safety procedures
applicable to your laboratory. |
 | Caution | Do not leave the EVM powered when unattended. |
WARNING: The circuit module has signal
traces, components, and component leads on the bottom of the board. This can result
in exposed voltages, hot surfaces, and sharp edges. Do not reach under the board
during operation.
WARNING: External Connections: All
external connections to the hardware must stay within the recommended operating
conditions and intended usage for all hardware and components connected in the
system.
CAUTION: The circuit module can be
damaged by overtemperature. To avoid damage, monitor the temperature during
evaluation and provide cooling.
CAUTION: Some power supplies can be
damaged by application of external voltages. If using more than one power supply,
check equipment requirements and use blocking diodes or other isolation techniques
to prevent damage to the equipment.
CAUTION: The communication interface is
not isolated on the EVM. Make sure that there is no ground potential between the
computer and the EVM. Be aware that the computer is referenced to the battery
potential of the EVM.