SLUUDG7A December 2025 – November 2026 MSPM33C321A , MSPM33C321A-Q1
The Global Security Controller (GSC) is a peripheral which can configure write erase protection on MSPM33. Any violation of the security property results in a non-maskable interrupt (NMI) which is logged into the EAM module. For other protection supported by GSC, please refer to the GSC chapter of the MSPM33 C3-Series 160MHz Microcontrollers technical reference manual.
For FLASH WEP configuration, FLASH is configured by sectors(0-64KB) or blocks(64KB-512KB). Please note the address below is physical address rather than logic address, which should be careful when doing FLASH bank swapping.
| FLASH BANK | Physical Address | Registers | Granular Control |
| BANK0 |
0x00000000-0x0000FFFF (0-64KB) |
FPC_WEPROTA0 | Sector(2KB) |
|
0x00010000- 0x0007FFFF (64KB-512KB) |
FPC_WEPROTB0 | Block(8 sectors, 16KB) | |
| BANK1 |
0x00080000-0x0008FFFF (0-64KB) |
FPC_WEPROTA1 | Sector(2KB) |
|
0x00090000- 0x000FFFFF (64KB-512KB) |
FPC_WEPROTB1 | Block(8 sectors, 16KB) | |
| DATA FLASH |
0x80000000-0x80007FFF (0-32KB) |
FPC_WEPROTA_DFLASH | Sector(2KB) |
If the device is 512KB dual bank device, then every bank will be 256KB rather than 512KB.