SLUUDG7A December 2025 – November 2026 MSPM33C321A , MSPM33C321A-Q1
The security attribution unit (SAU) can be used by the programmer to define regions of memories security. The final security level uses both the SAU configuration and the IDAU configuration. For determining a section of memories security level take the higher security level between the SAU and IDAU. For example if the SAU defines a region as secure and the IDAU defines a region as non-secure the region is defined as secure.
On the MSPM33 devices the SAU is built to support defining 8 regions as Secure, non-secure, or non-secure callable.