SLVSFJ6B November 2020 – October 2026 TPS27SA08
PRODUCTION DATA
Figure 9-4 shows the behavior of the TPS27SA08 device in this application when the MCU provides an enable pulse to beginning heating the resistive element. Shortly after the EN pin goes high, the load current begins to flow and the SNS pin measures the output current.
Figure 9-4 Heater Turn-on TimeBy measuring the voltage on the SNS pin, the TPS27SA08 device can communicate back to the system MCU what the load current is. Figure 9-5 shows that when the seat heater approaches full load and IOUT jumps from a low load current of 1A up to a 5A load current, the load step is mirrored on the SNS pin.
Figure 9-5 SNS Response During Heater Load StepOne common concern in these type of applications is that the heating element can accidentally lose connection, creating an open load situation. In this case, it is best for the TPS27SA08 device to recognize that the load has been removed and report a FLT to the MCU. Figure 9-6 shows the behavior of the TPS27SA08 device when there is no load attached. As soon as the DIAG_EN pin is engaged, the SNS output goes high and the ST output engages low. By monitoring these pins, the MCU can recognize there is a fault and notify the user that maintenance is required.
Figure 9-6 Open Load Detection If Heating Element is MissingImportantly, the TPS27SA08 device also protects the system in the event of a short circuit. Figure 9-7 shows the behavior of the device if it is enabled into a short circuit condition. The current is clamped to near the current limit threshold (ICL) until it hits an over temperature event, at which point the FET is turned off. In this way, the system is protected from unchecked overcurrent in the event of a short circuit.
Figure 9-7 Overcurrent Behavior During Short Circuit Event