SLVSFJ6B November 2020 – October 2026 TPS27SA08
PRODUCTION DATA
In the reverse supply condition, the switch automatically enables (regardless of EN status) to prevent power dissipation inside the MOSFET body diode. In many applications (for example, resistive load), the full load current can be present during reverse supply. To activate the automatic switch on feature, the SEL2 pin must have a path to module ground. This can be path 1 as shown below, or, if the SEL2 pin is unused, the path can be through RPROT to module ground.
Protection features (for example, thermal shutdown) are not available during reverse supply. Take care to verify that excessive power is not dissipated in the switch during the reverse supply condition.
There are two options for blocking reverse current in the system. Option 1 is to place a blocking device (FET or diode) in series with the supply. This blocks all current paths. Option 2 is to place a blocking diode in series with the GND node of the high-side switch. This method protects the controller portion of the switch (path 2), but it does not prevent current from flowing through the load (path 3). The diode used for Option 2 can share amongst multiple high-side switches.
Path 1 shown in Figure 8-3 is blocked inside of the device.