SLVSFJ6B November 2020 – October 2026 TPS27SA08
PRODUCTION DATA
Inverse current occurs when 0V < VBB < VOUT. In this case, current can flow from VOUT to VBB. A purely resistive load cannot cause inverse current. However, a capacitive or inductive load can cause inverse current. For example, if there is a significant amount of load capacitance and the VBB node has a transient droop, VOUT can be greater than VBB.
TPS27SA08 device does not detect inverse current. When the switch is enabled, inverse current passes through the switch. When the switch is disabled, inverse current can pass through the MOSFET body diode. The device continues operating in the normal manner during an inverse current event.