SLVSHM2B March 2025 – October 2026 TPS2HC120-Q1
PRODUCTION DATA
The quiescent current of the device during LPM, IQ,LPM, is a function of how many channels are active and is proportional to the load current meaning that the lower the load current during this time, the lower the quiescent current is. Additionally, since the digital core is disabled, the diagnostics like current sensing or open load detection are not available during this mode. If diagnostics are desired, the DIAG_EN pin can be enabled to exit LPM and return the part back to normal operation. Once DIAG_EN is disabled the device goes back into LPM after tSTBY. Similarly, the current limit mechanism is not active in the same manner as by definition the minimum current limit is higher than the entry point of LPM. However, the short-circuit protection is still in place to protect the device.
Below is the summary of the behavior of the device during LPM: