SLVSJ99 July 2025 TPLD2001-Q1
ADVANCE INFORMATION
The state machine macro-cell has 8 outputs into the connection mux. With an 8-byte RAM, users are able to set the behavior of the 8 outputs for each defined state, which could be seen as 8 parallel outputs that can be configured depending on the current state. Each of the 8 outputs are connection mux inputs that could be elsewhere in the design, such as an input into a LUT, D flip-flop, counter, or out to a GPO pin.
The state machine outputs can be updated in-system using the User Registers. For glitch-free operation, it is recommended to put the state machine in a reset while the state machine output bits are being modified.