SLVSJQ4 May 2026 TMF0020
PRODUCTION DATA
The Extended Read Memory command works similar to the Read Memory command, except for the 2-byte CRC that is transmitted at the end of each memory page. The host can read the FRAM memory by issuing the Extended Read Memory command (A5h), followed by the 2-byte address (LSB first). If the host issues an address greater than 1FC5h, the device sets the six most significant address bits to zero. The host can then read the data from either the address within the address range or the modified address until the end of a 32-byte page. At the end of the memory page, the host reads the 2-byte inverted CRC. If the host continues to read, the host receives the data corresponding to the beginning of next page and so on until the end address 1FC4h is reached. If the host continues to read further, the TMF0020 transmits 1s. The host can terminate the Read Memory command sequence by issuing a reset pulse.