A simplified application schematic for a 16-series
battery pack is shown in Figure 8-1, using the BQ76972-Q1 together with an external secondary protector, a host
microcontroller, and a communications transceiver. This configuration uses CHG and
DSG FETs in series, together with high-side PFET devices used to implement precharge
and predischarge functionality. Several points to consider in an implementation are
included below:
- The external NPN BJT used for the REGIN preregulator can be configured with its collector routed either to the cell battery stack or the middle of the protection FETs.
- A diode is recommended in the drain circuit of the external NPN BJT, which avoids reverse current flow from the BREG pin through the BJT base to collector in the event of a pack short circuit. This diode can be a Schottky diode if low voltage pack operation is needed, or a conventional diode can be used otherwise.
- A series diode is recommended at the BAT pin,
together with a capacitor from the pin to VSS. These components allow the device
to continue operating for a short time when a pack short circuit occurs, which
can cause the PACK+ and top-of-stack voltages to drop to approximately 0V. In
this case, the diode prevents the BAT pin from being pulled low with the stack,
and the device continues to operate, drawing current from the capacitor.
Generally operation is only required for a short time, until the device detects
the short circuit event and disables the DSG FET. A Schottky diode can be used
if low voltage pack operation is needed, or a conventional diode can be used
otherwise.
- The diode in the BAT connection and the diode in
the BJT collector must not be shared, since then the REG0 circuit might
discharge the capacitor on BAT too quickly during a short circuit event.
- The recommended voltage range on the VC0 to VC4
pins extends to –0.2V. This can be used, for example, to measure a differential
voltage that extends slightly below ground, such as the voltage across a second
sense resistor in parallel with that connected to the SRP and SRN pins.
- If a system does not use high-side protection
FETs, then the PACK pin can be connected through a series 10kΩ resistor to the
top of stack. The LD pin can be connected to VSS. In this case, the LD pin can
also be controlled separately, to wake the device from SHUTDOWN mode, such as
through external circuitry which holds the LD pin at the voltage of VSS while
the device stays in SHUTDOWN, and to be driven above a voltage of
VWAKEONLD to wake from SHUTDOWN.
- TI recommends using 100Ω resistors in series with
the SRP and SRN pins, and a 100nF with optional 100pF differential filter
capacitance between the pins for filtering. The routing of these components,
together with the sense resistor, to the pins must be minimized and fully
symmetric, with all components recommended to stay on the same side of the PCB
with the device. Optional 0.1μF filter capacitors can be added for additional
noise filtering at each sense input pin to VSS.
- Due to thermistors often being attached to cells
and possibly needing long wires to connect back to the device, it can be helpful
to add a capacitor from the thermistor pin to the device VSS. However, it is
important to not use too large of a value of capacitor, since this will affect
the settling time when the thermistor is biased and measured periodically. To
keep the time constant of the circuit < 5% of the measurement time. When
Settings:Configuration:Power Config[FASTADC] = 0, the
measurement time is approximately 3ms, and with [FASTADC] = 1 the
measurement time is halved to approximately 1.5ms. When using the 18kΩ pullup
resistor with the thermistor, the time constant will generally be less than
(18kΩ) × C, so a capacitor less than 4nF is recommended. When using the 180kΩ
pullup resistor, the capacitor must be less than 400pF.
- The integrated charge pump generates a voltage on
the CP1 capacitor, requiring approximately 60ms to charge up to approximately
11V when first enabled, when using the recommended 470nF capacitor value. When
the CHG or DSG drivers are enabled, charge redistribution occurs from the CP1
capacitor to the CHG and DSG capacitive FET loads. This will generally result in
a brief drop in the voltage on CP1, which is then replenished by the charge
pump. If the FET capacitive loading is large, such that at FET turn-on the
voltage on CP1 drops below an acceptable level for the application, then the
value of the CP1 capacitor can be increased. This has the drawback of requiring
a longer startup time for the voltage on CP1 when the charge pump is first
powered on, and so must be evaluated to ensure it is acceptable in the system.
For example, if the CHG and DSG FETs are enabled simultaneously and the combined
gate capacitance is approximately 400nF, then changing CP1 to a value of 2200nF
will result in the 11V charge pump level dropping to approximately 9V, before
being restored to the 11V level by the charge pump.
A full schematic of a basic monitor circuit based
on the pin-compatible BQ76952 for a 16-series battery pack is shown below. Section 8.8.2 shows the board
layout for this design.