This value depends on the cell chemistry and the
load requirements of the system. For example, to support a minimum
battery voltage of 20V using Li-CO2 type cells with a cell minimum
voltage of 3V, there needs to be at least 7-series cells.
The BQ76972-Q1 device is designed for use with high-side NFET protection (low-side protection NFETs can be used by leveraging the DCHG / DDSG signals)
The configuration must be selected for series
versus parallel FETs, which can lead to different FET selection for
charge versus discharge direction.
These FETs must be rated for the maximum:
Voltage, which
must be approximately 5V (DC) to 10V (peak) per series
cell.
Current, which
must be calculated based on both the maximum DC current and the
maximum transient current with some margin.
Power
Dissipation, which can be a factor of the RDS(ON) rating of the
FET, the FET package, and the PCB design.
The overdrive level of the BQ76972-Q1 device
charge pump must be selected based on RDS(ON) requirements for the
protection FETs and the voltage handling requirements. If the FETs are
selected with a maximum gate-to-source voltage of 15V, then the 11V
overdrive mode within the BQ76972-Q1 device can be used. If the FETs are
not specified to withstand this level, or there is a concern over gate
leakage current on the FETs, the lower overdrive level of 5.5V can be
selected.
Sense resistor selection
The resistance value must be selected to maximize
the input range of the Coulomb counter but not exceed the absolute
maximum ratings, and avoid excessive heat generation within the
resistor.
Using the normal
maximum charge or discharge current, the sense resistor = 200mV
/ 20.0A = 10mΩ maximum.
A short circuit
discharge current of 80A, the recommended maximum SRP, SRN
voltage of approximately 0.75V, and the maximum SCD threshold of
500mV, the sense resistor must be below 500mV / 80A= 6.25mΩ
maximum.
Further tolerance analysis (value tolerance,
temperature variation, and so on) and PCB design margin must also be
considered, so a sense resistor of 1mΩ is suitable with a 50ppm
temperature coefficient and power rating of 1W.
The REG1 is selected to provide the supply for an
external host processor, with output voltage selected for 3.3V.
The NPN BJT used for the
REG0 preregulator must be selected to support the maximum
collector-to-emitter voltage of the maximum charging voltage of 34V. The
gain of the BJT must be chosen so it can provide the required maximum
output current with a base current level that can be provided from the
BQ76972-Q1 device.
The BJT must support
the maximum current expected from the REG1 (maximum of 45mA, with short
circuit current limit of up to approximately 80mA).
A diode can optionally be
included in the collector circuit of the BJT, avoid reverse current flow
from BREG through the base-collector junction of the BJT to PACK+ during
a pack short circuit event. This diode can be seen in Figure 8-2 at D2.
A large resistor (such as
10MΩ) is recommended from BREG to VSS, to avoid any unintended leakage
current that can occur during SHUTDOWN mode.