SLVSNS8 September   2026 TMUXS1306A

ADVANCE INFORMATION  

  1.   1
  2. 1 Features
  3. 2 Applications
  4. 3 Description
  5. 4 Device Comparison Table
  6. 5 Pin Configuration and Functions
  7. 6 Specifications
    1. 6.1  Absolute Maximum Ratings
    2. 6.2  ESD Ratings
    3. 6.3  Recommended Operating Conditions
    4. 6.4  Thermal Information: TMUXS1306A
    5. 6.5  Thermal Information: TMUXS1307A
    6. 6.6  Electrical Characteristics
    7. 6.7  Logic and Dynamic Characteristics
    8. 6.8  Timing Characteristics
    9. 6.9  Injection Current Coupling
    10. 6.10 SPI Timing Characteristics (5.5V)
    11. 6.11 SPI Timing Characteristics (3.3V)
    12. 6.12 SPI Timing Characteristics (2.7V)
    13. 6.13 SPI Timing Characteristics (1.8V)
  8. 7 Parameter Measurement Information
    1. 7.1  On-Resistance
    2. 7.2  Off-Leakage Current
    3. 7.3  On-Leakage Current
    4. 7.4  Transition Time
    5. 7.5  Break-Before-Make
    6. 7.6  tON(EN) and tOFF(EN)
    7. 7.7  Charge Injection
    8. 7.8  Off Isolation
    9. 7.9  Crosstalk
    10. 7.10 Bandwidth
    11. 7.11 Injection Current Control
  9. 8 Detailed Description
    1. 8.1 Overview
    2. 8.2 Functional Block Diagram
    3. 8.3 Feature Description
      1. 8.3.1 Bidirectional Operation
      2. 8.3.2 Rail-to-Rail Operation
      3. 8.3.3 1.8V Logic Compatible Inputs
      4. 8.3.4 Fail-Safe Logic
      5. 8.3.5 Injection Current Control
    4. 8.4 Device Functional Modes
      1. 8.4.1 SPI Operation
        1. 8.4.1.1 Auto Cycle Mode
        2. 8.4.1.2 Address Mode
        3. 8.4.1.3 Burst Mode
        4. 8.4.1.4 Daisy Chain Mode
        5. 8.4.1.5 Software Reset
  10. 9  TMUXS1306A Register Map
  11. 10 TMUXS1307A Register Map
  12. 11Application and Implementation
    1. 11.1 Application Information
    2. 11.2 Typical Application
      1. 11.2.1 Design Requirements
      2. 11.2.2 Detailed Design Procedure
    3. 11.3 Power Supply Recommendations
    4. 11.4 Layout
      1. 11.4.1 Layout Guidelines
      2. 11.4.2 Layout Example
  13. 12Device and Documentation Support
    1. 12.1 Documentation Support
      1. 12.1.1 Related Documentation
    2. 12.2 Receiving Notification of Documentation Updates
    3. 12.3 Support Resources
    4. 12.4 Trademarks
    5. 12.5 Electrostatic Discharge Caution
    6. 12.6 Glossary
  14. 13Revision History
  15. 14Mechanical, Packaging, and Orderable Information
    1. 14.1 Tape and Reel Information
    2. 14.2 Mechanical Data

Injection Current Control

On a high level, Injection current control is a feature that prevents an overvoltage event on an unactive channel from impacting the signal on an active one. The pin that experiences an overvoltage event will be held at VDD+VT, where VT ≅ 0.6V. The excess current caused by clamping this voltage will flow through an internal circuit that must remain within the current specifications of the device. By doing this, the device can prevent the excess current from injecting into the ON-channel causing errors in measurement. Injection current is the current that is being forced into a pin by an input voltage (VIN) higher than the positive supply (VDD + ∆V) or lower than ground (VSS). The current flows through the input protection diodes into whichever supply of the device is potentially compromising the accuracy and reliability of the system. Injected currents can come from various sources depending on the application.

  • Harsh environments and applications with long cabling, such as in factory automation and automotive systems, may be susceptible to injected currents from switching or transient events.
  • Other self-contained systems can also be subject to injected current if the input signal is coming from various sensors or current sources.

Injected Current Impact: typical CMOS switches have ESD protection diodes on the inputs and outputs. These diodes not only serve as ESD protection but also provide a voltage clamp to prevent the inputs or outputs going above VDD or below GND and VSS. When current is injected into the pin of a disabled signal path, a small amount of current goes through the ESD diode but most of the current goes through conduction to the drain. If forward diode voltage of the ESD diode (VF) is greater than the PMOS threshold voltage (VT), then the PMOS of all OFF switches turns ON and there would be undesirable subthreshold leakage between the source and the drain that can lift the OFF source pins up also. Figure 8-1 shows a simplified diagram of a typical CMOS switch and associated injected current path.

TMUXS1306A TMUXS1307A Simplified Diagram of Typical CMOS Switch and Associated Injected Current PathFigure 8-1 Simplified Diagram of Typical CMOS Switch and Associated Injected Current Path

It is quite difficult to cut off these current paths. The drain pin can never be allowed to exceed the voltage above VDD by more than a VT. Analog pins can be protected against current injection by adding external components like a Schottky diode from the drain pin to ground to clamp the drain voltage at < VDD + VT and cut off the current path.

Change in RON due to Current Injection: because the ON resistance of the enabled FET switch is impacted by the change in the supply rail, when the drain pin voltage exceeds the supply voltage by more than a VT, an error in the output signal voltage can be expected. This undesired change in the output can cause issues related to false trigger events and incorrect measurement readings, potentially compromising the accuracy and reliability of the system. As shown in Figure 8-2, S2 is the enabled signal path that is conducting a signal from S2 pin to D pin. Because there is an injected current at the disabled S1 pin, the voltage at that pin increases above the supply voltage and the ESD protection diode is forward biased, shifting the power supply rail. This shift in supply voltage alters the RON of the internal FET switches, causing a ∆V error on the output at the D pin.

TMUXS1306A TMUXS1307A Injected Current Impact on
                        RONFigure 8-2 Injected Current Impact on RON

To avoid the complications of added external protection to your system, the TMUXS1306A and TMUXS1307A devices have an internal injection current control feature which eliminates the need for external diode and resistor networks typically used to protect the switch and keep the input signals within the supply voltage. The internal injection current control circuitry allows the signals on the disabled signal paths to exceed the supply voltage without affecting the signal of the enabled signal path. The injection current control circuitry also protects the TMUXS130xA from currents injected into disabled signal paths without impacting the enabled signal path, which typical CMOS switches do not support. Additionally, the TMUXS1306A and TMUXS1307A do not have any internal diode paths to the supply pin, which eliminates the risk of damaging components connected to the supply pin or providing unintended power to the system supply rail. For a simplified diagram that shows one signal path for the TMUXS130xA devices and the associated injection current circuit, refer to Section 8.2.

TMUXS1306A TMUXS1307A Simplified Diagram of Injection Current ControlFigure 8-3 Simplified Diagram of Injection Current Control

The injection current control circuitry is independently controlled for each source or drain pin (Sx or D). The control circuitry for a particular pin is enabled when that input is disabled by the logic pins and the injected current causes the voltage at the pin to be above VDD or below GND. The injection current circuit includes an FET to shunt the undesired current to GND in the case of overvoltage or injected current events. Each injection current circuit is rated to handle up to 50mA; the device, however, can support a maximum current of 100mA at any given time. Depending on the system application, a series limiting resistor may be needed and must be sized appropriately. Figure 8-3 shows the TMUXS130xA protection circuitry with an injected current at an input pin.

TMUXS1306A TMUXS1307A Injected Current at Input PinFigure 8-4 Injected Current at Input Pin

Figure 8-5 shows an example of using a series limiting resistor in the case of an overvoltage event.

TMUXS1306A TMUXS1307A Over-Voltage Event with Series ResistorFigure 8-5 Over-Voltage Event with Series Resistor

For the injection current control circuitry to be active the voltage at the source or drain pins is greater than VDD, or less than GND. With this requirement met, the protection FET will be turned on for any disabled or enabled signal path and shunt the pin to GND. In this event, a series resistor is needed to limit the total current injected into the device to be less than 100mA. Three example scenarios are outlined in the following sections.