Use the following instructions to perform the overvoltage protection test on channel 1:
- Remove the input TVS diodes.
- Place jumper J4 in position 1-2 and J7 in a good position to set the required
OVLO threshold as per Table 4-3. For example, consider setting 1-2 to set threshold as 13.8 V.
- Set the input supply voltage VIN to 12 V and current limit of 9 A. Apply the supply between VIN1 and PGND1 at connector J2 and enable the power supply.
- Increase the input supply VIN from 12 V to 15 V and observe the waveforms using
an oscilloscope.
Figure 5-6 shows overvoltage response of TPS25948 on the TPS25948EVM eFuse evaluation board.