SLVUCP4A November 2023 – August 2025
This section describes applications for the TPS25730.
The TPS25730 is a PD controller that enables the sinking of power to the system through a USB-C connector using the USB-PD specification, as shown in Figure 1-1. Due to the ability to configure power settings by voltage dividers at the ADCINx pins, no EEPROM is needed, which reduces BOM cost and saves board space. Additionally, no software or GUI is required, minimizing development time.
With the ADCINx pins configured the desired settings, as described in Section 2.7, the TPS25730 sinks the negotiated amount of power through the PPHV pin from a USB-PD capable source.
How this negotiation occurs is detailed in the Universal Serial Bus Power Delivery Specification. This specification can be accessed at USB Power Delivery.
In broad terms: