SLVUCR9C August   2023  – April 2025 TPS2HCS10-Q1

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Assembly Instructions
    2. 2.2 Revision Differences
    3. 2.3 Jumper Information
    4. 2.4 Interfaces
    5. 2.5 Test Points
    6. 2.6 Transient Testing
  9. 3Software
    1. 3.1 Software Usage
      1. 3.1.1  Command Center View
      2. 3.1.2  I2T Tuner
      3. 3.1.3  Device Settings
      4. 3.1.4  Channel Settings
      5. 3.1.5  Console View
      6. 3.1.6  Log View
      7. 3.1.7  Importing/Exporting
      8. 3.1.8  Firmware Updates
      9. 3.1.9  Persist Settings
      10. 3.1.10 Language Settings
    2. 3.2 Software Development
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Revision History

Channel Settings

The Channel Settings tab shows a list of settings that are specific to channels and not to the device as a whole. As many of the supported high-side switches are multi-channel devices, the Channel Number drop-down box is used to change between settings for different channels. Many of these settings are duplicated from the command center view, however changing them in one tab also updates the setting in the other tab. Likewise, the I2T Parameters box contains parameters that are the same as those configured in the I2T Tuner tab. Refer to the device data sheet for the meaning/configuration values of each parameter.

The Capacitive Charging box controls the capacitive charging mode that the device is set to:

TPS2HCS10-Q1 Channel Settings Figure 3-13 Channel Settings