SLVUDB0A August   2025  – October 2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 ADS9324EVM Quick Start Guide
    2. 2.2 Analog Interface
      1. 2.2.1 ADC Input SMA Connections
      2. 2.2.2 Voltage Reference
    3. 2.3 Digital Interface and Clock Inputs
      1. 2.3.1 Digital Interface Connections
      2. 2.3.2 Level Translators
    4. 2.4 Power Supplies
      1. 2.4.1 USB Power and When to Power the Board Externally
  7. 3Software
    1. 3.1 ADS9324EVM Software Installation
      1. 3.1.1 USB Driver Installation
    2. 3.2 ADS9324EVM Software
      1. 3.2.1 Using Configuration Tab
      2. 3.2.2 Using the Data Capture Tab
      3. 3.2.3 Using the Linearity Analysis Tab
      4. 3.2.4 Using the Histogram Analysis Tab
  8. 4Hardware Design Files
    1. 4.1 Schematics
      1. 4.1.1 ADS9324EVM Schematics
    2. 4.2 Layout
    3. 4.3 Bill of Materials (BOM)
      1. 4.3.1 ADS9324EVM Bill of Materials (BOM)
  9. 5Additional Information
    1. 5.1 Trademarks
  10. 6Related Documentation
  11. 7Revision History

ADS9324EVM Software Installation

This section details the installation and operation of the ADS9324EVM software graphical user interface (GUI). This software requires the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software (as shown in Figure 3-1) is to download the latest version of the EVM GUI installer as per Table 3-1.

Table 3-1 EVM GUI Installers
EVMSoftware Download Link
ADS9324EVMADS9324EVM-GUI

Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements.

Note: The GUI installer and GUI buttons can differ slightly depending on which specific GUI is being installed.
ADS9324EVM Initial Software InstallationFigure 3-1 Initial Software Installation

Next, the installer prompts the user to create a desktop icon and summarize the installation plan. Clicking Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. Figure 3-2 shows these steps.

ADS9324EVM Installation ProcessFigure 3-2 Installation Process