SLVUDB9A July 2025 – November 2026
In addition to software provided by TI there are some additional software packages required to evaluate the ADC.
FTDI D3xx Driver
Download
WU_Driver_Installers.7z - FTDI D3XX v1.4.1.0 — Windows Update Driver Installers (required version)
Extract the Archive
The .7z format requires 7-Zip or a compatible tool:
Right-click the file
Select 7-Zip → Extract Here
Installation Steps
Extract WU_Driver_Installers.7z to a folder of your choice.
Inside the extracted folder, locate the installer for your Windows version:
For Windows 10/11 x64: run the x64 installer
Run the installer as Administrator and follow the prompts.
Connect the TSW14J58 board's USB3-A cable to a USB 3.0 port on your PC (blue port or marked SS).
Open Device Manager and verify the device appears as TSW14J58 under Universal Serial Bus controllers.
Reboot after installation.
Important Notes
USB 3.0 is required. Plugging into a USB 2.0 port will cause device enumeration to fail.
If the device does not enumerate after driver install:
Try a different USB3 port or cable
Ensure the board is fully powered on before connecting
Plug USB3 directly into PC and not through any USB hubs as this may also cause issues