SLVUDB9A July 2025 – November 2026
This tab lets the user configure the number of active channels used by the ADC with the constraint that channel A must always be active and only power of two number of channels are valid. The input termination for each ADC channel is also programmable here with valid values differing depending on device in use. The nyquist zone of operation is also selectable here there are two default opions picked here, if operation in a higher nyquit is desired a custom mode is avlaible in the run time option see NLC tab. This will affect device non-linearity performance.
Figure 4-1 Static Configuration ->
AIN