SLVUDB9A July 2025 – November 2026
The ADC3xRF7x has four analog inputs and the EVM routes all four as length matched signals. The default comes configured as single ended inputs that are AC couple and then SE-DIFF converted using the on board balun. There is also space on the EVM for a matching network to experiment with different matching networks depending on the application requirements.
The input networks are slightly different across the three part variants, the ADC34RF72 uses the BAL003SMG from Marki Microwave and the ADC34RF75 and ADC32RF77 use the BAL006SMG from Marki Microwave. The ADC32RF77 also only populates two out of the four input networks as it is only a two channel device whereas the ADC34RF72 and ADC34RF75 populate all four analog inputs.
The EVM can also be configured to accept an external differential signal with the following modifications. For components to bypass on board baluns, see Figure 6-3 through Figure 6-6.
Figure 6-3 ADC3xRF72 EVM Input A Analog Input Schematic Snippet
Figure 6-4 ADC3xRF72 EVM Input B Analog Input Schematic Snippet
Figure 6-5 ADC3xRF72 EVM Input C Analog input Schematic Snippet
Figure 6-6 ADC3xRF72 EVM Input D Analog Input Schematic Snippet