| General Issues | - Verify test setup shown in Section 2
and repeat “ADC EVM quick start” section to verify basic
functionality.
- Check power supply to ADC EVM and TI Capture Card. If Power good LEDs on ADC EVM are not lit up then there is likely a power supply issue.
- Check signal and clock connections
- Make sure that the FMC connector is tightly secured
|
| TI Capture Card cannot connect in JESD Controller Server Application | - Make sure that all steps to setup 3rd
party software are followed in Section 2.5.
- Make sure that the USBC path is directly plugged into the PC and does not go through and USB hubs.
- Using FT Prog check for USB 2.0 connection shows a usb connection with usb descriptor "TSW14J58_CTRL"
- Check device manager to ensure that the USB 3.0 path shows up as "TSW14J58" under the Universal Serial Bus device.
- Additonaly ensure in device manager that the driver for the TSW14J58 is version 1.4.0.1
- If connection of board in JESD controller server is still unsuccessfu, uninstall and reinstall the application
|
| ADC EVM cannot connect in GUI | - Verify that the USB cable and daughter card are making solid connection.
- Using FT_Prog verify that the ADC FTDI handle is found and matches one of the valid options "ADC34RF72EVM_RevA", "ADC32RF77EVM_RevA", "ADC34RF75EVM_RevA", "ADC34RF72EVM_RevC", "ADC32RF77EVM_RevC", "ADC34RF75EVM_RevC"
|
| ADC EVM fails programming | - Make sure that device clock to ADC has enough power to the EVM (9dBm) and the frequency matches what is programmed in the GUI.
- Check that the resetb signal is not held low. Using the multimeter probe RSTb signal located on the GPIO header. This signal reads approximately 1.8V indicating the ADC is not being held in reset. If this is not the case the EVM can be damaged or broken.
|
| ADC Link fails to come up | - In FPGA tab of the ADC EVM GUI there are a number of LEDs to indicate the FPGAs status. Refer to this and the corresponding table entries below.
|
| FPGA Connect LED not lit up | See above table Entry "TI Capture Card cannot connect in GSPS FPGA Server Application" |
| FPGA Programmed LED not lit up | - Verify that power supply meets the criteria of 6V, 6A. Programming the FPGA is one of the highest current draws on the FPGA. Check that during this time the power supply is not hitting its current compliance.
|
| FPGA PLLs Unlocked | - Verify that EVM hardware is setup as shown in
Section 2.6
and reference clock to the EVM is at least 6dBm and the
frequency matches what is selected in the GUI for the ADC sample
frequency.
- Verify that ADC Clock and reference clock are phase locked to each other with 10MHz signal.
- Using Oscilloscope probe on resistor R62 and make sure that frequency matches what is shown in the ADC EVM GUI in the Bringup>JESD tab in the “FPGA Ref Clock” box.
|
| ADC Lanes Unlocked | - Verify that programmed JESD params in the GSPS FPGA Server match what is shown in the ADC EVM GUI in the Bringup>JESD tab.
- Probe resistor R204 and make sure that ADC SYSREF signal is present and matches the frequency shown in the Bringup>JESD tab in the “SYSREF” box.
|
| ADC Lanes Lock but release delay is stuck at zero | - Probe resistor R204 and make sure that ADC SYSREF signal is present and matches the frequency shown in the Bringup>JESD tab in the “SYSREF” box.
|
| ADC Lane Buffer Overflow | - Probe resistor R204 and make sure that ADC SYSREF signal is present and matches the frequency shown in the Bringup>JESD tab in the “SYSREF” box.
- Verify that ADC Clock and reference clock are phase locked to each other.
|
| Sub Optimal Performance | - Verify signal quality of both clock and ADC inputs as these directly limit the ADCs performance.
- Make sure that the bandpass filters are used for both ADC clock and any inputs.
|