SLVUDL1A November 2025 – December 2025
Connect the input voltage to the J1 connector and verify that the positive and negative supply is connected appropriately. The positive and negative terminals are marked on the board. The sense connection for the input supply is through the TP1 and TP7 test points, respectively. This is useful when doing efficiency calculations as this verifies that the resistive losses to the board are considered and the losses calculated are related to the board and the LMG210XR044 half bridge.
NOTE
Please remove the TVS Diode (D6) connected to the Input Connector if the Input Voltage applied exceeds 75V.
The output load is connected to the J2 connector. The positive and negative sense signals are TP2 and TP3, respectively.