Use the following steps for communication
verification:
- In the EVM software, click the
Read Register button.
- Verify that the GUI reads
Device ACK OK in the top right corner.
- In the Field View (see Figure 3-3), make the following changes as necessary:
- Set WATCHDOG to Disable
- Set 16 bit registers to the
following
- Check Charge Enable
- Uncheck Enable Termination