SLVUDQ1 May 2026
TAS2573EVM has been designed such that the dummy load or speaker load connected to the device can be measured very accurately directly from the device pin including board parasitic and connector contact resistance using 4-wire method in digital multimeter. Pin headers have been provided to be able to connect digital multimeter in 4-wire mode as shown in Figure 2-12.
For channel-1: Connect HI of DMM to pin-1 and HI_SNS of DMM to pin-2 of TP13 test point.
Connect LO of DMM to pin-2 and LO_SNS of DMM to pin-1 of TP15 test point.
For channel-2: Connect HI of DMM to pin-1 and HI_SNS of DMM to pin-2 of TP28 test point.
Connect LO of DMM to pin-2 and LO_SNS of DMM to pin-1 of TP30 test point.
Figure 2-12 Load DC Resistance Measurement in 4-Wire Mode Using Digital
Multimeter