SLVUDQ1 May 2026
Since TAS2573EVM is a dual-mono EVM, each channel has a speaker output connector.
SPK1_P and SPK1_N are the outputs for channel-1 device, whereas SPK2_P and SPK2_N are the outputs for channel-2. Two different types of connectors have been provided: horizontal banana connectors and push horizontal sockets, to be able to connect speaker or dummy load with fly-wires or male banana connectors. These can also be used to connect to an audio analyzer analog input cable for performance measurements.
Channel-1 output connectors as shown in Figure 2-10:
Channel-2 output connectors as shown in Figure 2-10: