SLVUE20 September 2026
Each TUSB2514EVM is equipped with an onboard EEPROM/socket placeholder, U2. A small I2C EEPROM can be installed to set the configuration registers as defined in the TUSB2514 data manual (SLVSL35). In its default setting, the EVM does not have an EEPROM installed and instead uses the configuration inputs to determine any optional settings of the TUSB2514. The EEPROM interface defaults to programmable (not write-protected) so that any installed EEPROM’s contents may be modified to test various settings. If an EEPROM data change is required, the values may be changed using the register access methods outlined in the TUSB2514 data sheet. In addition, a Microsoft® Windows® based EEPROM utility is available upon request.