SLVUE20 September 2026
Each downstream VBUS output has a 150μF bulk capacitor as recommended by the TPS20xxC and TPS20xxC-2 Current Limited, Power-Distribution Switches datasheet to prevent in-rush current events on the downstream devices. In addition, there are ferrite beads and small capacitors on the VBUS lines to reduce noise and address ESD/EMI concerns. The TUSB2514EVM also implements optional isolation using two small noise-filtering capacitors and a 1MΩ resistor between the earth ground of each connector and the digital ground of the EVM. This is not a requirement but must be used if ground isolation is needed.