SNAS758A February 2025 – June 2025 HDC3120
PRODUCTION DATA
Rehydration restores the baseline performance of the humidity sensor after high-temperature exposure, such as solder reflow. During reflow, the sensing polymer can temporarily lose moisture, causing a short-term shift in readings. Rehydration allows the polymer to re-equilibrate, improving stability and accuracy, especially at high humidity levels.
Texas Instruments recommends the following accelerated rehydration routine:
This accelerated routine fully saturates the sensing polymer and aligns the polymer with factory calibration, providing accurate and consistent performance in high-RH environments. This procedure quickly and thoroughly restores the equilibrium of the polymer, enhancing measurement accuracy; particularly at RH levels above 70%, where precision is most sensitive to sensor saturation.
Alternatively, the HDC3120 can be rehydrated using a standard room-condition routine:
Room Condition Rehydration: 25 °C, 40–50% RH for 5 days
However, room-condition rehydration can leave the polymer under-saturated, leading to slightly lower RH readings at high-humidity test points. This under-saturation can result in measurements that fall outside of specification. Figure 8-5 illustrates the performance differences between the two rehydration routines.
The error introduced by room-condition rehydration often self-corrects if the device is exposed to high humidity (>30 minutes) during actual testing. Nevertheless, this behavior is less predictable, and measurement accuracy can be temporarily affected. Therefore, wherever possible, Texas Instruments recommends the accelerated rehydration routine for more reliable and predictable sensor performance.