SNAS855H November 2023 – October 2026 LMKDB1102 , LMKDB1104 , LMKDB1108 , LMKDB1112 , LMKDB1120
PRODUCTION DATA
In the recommended power down sequence, PWRDN# is asserted while input clocks are valid. Make sure to hold the PWRDN# pin at low level for two consecutive rising edges of the input clock cycle. As a result, all clock outputs are muted to low/low (OUTx_P = Low, OUTx_N = Low) without a glitch. Following any other sequence brings the device to an undefined mode and can cause glitches or invalid outputs - for example, if PWRGD/PWRDN# is pulled low after the input clock is removed, the device enters a glitch state, where the output gets stuck low (but only if the PWRGD/PWRDN# pin is not moved back from low to high before the CLKIN signal is turned back on). If PWRGD/PWRDN# is pulled back to high before the CLKIN signal returns, there are no issues.