SNAU283 October 2022
Click Select Device → Clock Generator/Jitter Cleaner (Dual Loop) → LMK04368-EP.
After start-up, the TICS Pro will load to the last used device. A recent history of used devices can be quickly accessed under the File menu. To load a new device, click Select Device from the menu bar, select the subgroup, then select the device to load.
Figure 5-1 Selecting the
LMK04368-EP.