SNAU292 August 2023
From the top-menu, click Default Configuration → 3200MHz Buffer Mode. This automatically loads the buffer mode profile.
If termination is not applied on all output pins, then manually disable the unused outputs using the CHx_EN fields (to completely power down unused channels) or the CLKOUTx_EN, SYSOUTx_EN, and LOGICLK_EN/LOGISYS_EN fields (to power down output buffers only). Powering down unused channels greatly reduces current consumption, and for the logic clocks in particular can reduce spurious interference.After the profile is loaded and required any changes have been made, click USB Communications → Write All Registers to program the device.
In all of the following plots, the blue trace is the 3.2GHz reference clock from SMA100B and the black trace is the output clock from the device.
Figure 4-1 Buffer Mode Signal Analyzer
PlotTo activate the multiplier or the divider, change the CLK_MUX field to specify divider or multiplier modes, and change the CLK_DIV and CLK_MULT fields to specify the frequency scaling factor.
Figure 4-2 Divide-by-2 Mode Signal
Analyzer Plot
Figure 4-3 Multiplier x4 Mode Signal
Analyzer Plot