SNAU292 August   2023

 

  1.   1
  2.   Description
  3.   Features
  4.   Applications
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Setup
      1. 2.1.1  Evaluation Setup Requirement
      2. 2.1.2  Connection Diagram
      3. 2.1.3  How to Enable Full SPI Control
      4. 2.1.4  Power Requirements
      5. 2.1.5  Pin Mode Strapping
      6. 2.1.6  Reference Clock
      7. 2.1.7  Output Connections
      8. 2.1.8  Header Information
      9. 2.1.9  Default Configuration
      10. 2.1.10 How to Generate SYSREF
      11. 2.1.11 Multiplier Mode Example
      12. 2.1.12 Divider Mode Example
      13. 2.1.13 Hybrid Mode: SPI and Pin Mode
  8. 3Software
    1. 3.1 Software Installation
    2. 3.2 Software Description
    3. 3.3 USB2ANY Interface
  9. 4Implementation Results
    1. 4.1 Buffer, Divider, and Multiplier Modes
    2. 4.2 SYSREF Generation
    3. 4.3 SYSREF Delay Generators
  10. 5Hardware Design Files
    1. 5.1 Schematic
    2. 5.2 PCB Layout
    3. 5.3 PCB Layer Stack-Up
    4. 5.4 Bill of Materials
  11. 6Additional Information
    1. 6.1 Troubleshooting Guide
      1. 6.1.1 General Guidance
      2. 6.1.2 If Output Is Not Seen on CLKOUT
      3. 6.1.3 If Device Features Are Not Active
      4. 6.1.4 If Multiplier Frequency Is Not Accurate
      5. 6.1.5 If Divider Frequency Is Not Accurate
      6. 6.1.6 If SYSREF Is Not Observed
    2. 6.2 Trademarks

USB2ANY Interface

The on-board USB2ANY interface provides a bridge between TICS Pro software and the LMX1404-EP device. When the on-board USB2ANY controller is first connected to a PC, or if the firmware revision for the controller does not match with the version used by TICS Pro, a firmware update to the controller is required.

  1. Connect the USB cable from the PC to the EVM. The USB interface provides the necessary power to enable the on-board USB2ANY controller.
  2. After Windows has set up a USB device, run TICS Pro in the PC.
  3. The next screen looks like the image below.
    LMX1404EPEVM  Firmware
                            Update Figure 3-1 Firmware Update
  4. Click OK, then the screen looks like the image below. Click Update Firmware.
    LMX1404EPEVM  Firmware
                            Loader Figure 3-2 Firmware Loader
  5. Then the screen below appears.
    LMX1404EPEVM  Firmware Update
                            Complete Figure 3-3 Firmware Update Complete
  6. Click the Close button to close the window.
  7. A TICS Pro default device pops up. Check to make sure that we get a green light on Connection Mode at the bottom of the GUI.
    LMX1404EPEVM  Connection
                            Mode Figure 3-4 Connection Mode
  8. Go to the menu bar, click USB communications, then select Interface.
    LMX1404EPEVM  USB
                            Communications Figure 3-5 USB Communications
  9. Click the Identify button, the LED in the USB2ANY interface flashes.
    LMX1404EPEVM  Identify USB2ANY
                            Controller Figure 3-6 Identify USB2ANY Controller
  10. Now, the USB2ANY is ready to use. Click the Close button to close the window.