SNLS787 September 2025 TDP2004-Q1
PRODUCTION DATA
The TDP2004-Q1 can also be configured by reading from EEPROM. To enter into this mode MODE pin must be set to L1. The EEPROM load operation only happens once after the initial powerup of the device. If the TDP2004-Q1 is configured for SMBus Controller mode, the device remains in the SMBus IDLE state until the READ_ENn pin is asserted to LOW. After the READ_ENn pin is driven LOW, theTDP2004-Q1 becomes an SMBus Controller and attempts to self-configure by reading the device settings stored in an external EEPROM (SMBus 8-bit address 0xA0). When the TDP2004-Q1 has finished reading from the EEPROM successfully, the device drives the DONEn pin LOW. SMBus/I2C Target operation is available in this mode before, during, or after EEPROM reading. Note: during EEPROM reading, if the external SMBus/I2C Controller wants to access TDP2004-Q1 registers, the external controller must support arbitration.
When designing a system for using the external EEPROM, the user must follow these specific guidelines:
Multiple TDP2004-Q1 can be cascaded to read from single EEPROM. Tie the READ_ENn pin of the first device low (GND) to automatically initiate EEPROM read at power up. DONEn of the first device can be fed into READ_ENn of the next device with 4.7kΩ pullup resistors. Leave the DONEn pin of the final device floating, or connect the pin to a micro-controller input to monitor the completion of the final EEPROM read.