To overcome high power loss disadvantages of the
diode design, as shown in Figure 2-2, using MOSFET which has much lower voltage drop or power loss (because of low
Rdson) is an alternative. However, there still are some drawbacks,
- MOSFET is not a standalone design, the ON or OFF
needs MCU control.
- MCU control needs power from PV panel, if PV
panel is badly damaged or fully covered by shadow, then MCU is not able to work
then MOSFET cannot be correctly turned ON.
- In cases that MCU does not work or is out of
control, the MOSFET is not turned ON, now the bypass path is the parasitic
diode. But parasitic diode cannot bear large current and can accumulate huge
amounts of heat that finally has risk of causing fire.