SNOAAA8 April   2025 LM74610-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 What is MLPE
    2. 1.2 Why, When, Where Needs MLPE
    3. 1.3 What is Solar Power Optimizer
    4. 1.4 Solar Power Optimizer Working Principle
    5. 1.5 Output Bypass Function of Solar Power Optimizer
  5. 2Traditional Designs of the Bypass Circuit
    1. 2.1 Design 1 - Using P-N Junction Diode or Schottky Diode
    2. 2.2 Design 2 - Using MOSFET
  6. 3New Design of the Bypass Circuit
    1. 3.1 Requirements on Bypass Circuit
    2. 3.2 Using Ideal Diode Controller LM746x0-Q1
    3. 3.3 Challenges of Using Ideal Diode Controller
    4. 3.4 Working Principle of LM746x0-Q1 Reverse Voltage Range Extension
  7. 4Bench Test and Result
  8. 5Summary
  9. 6References

Working Principle of LM746x0-Q1 Reverse Voltage Range Extension

First of all, understand what is depletion MOSFET. Distinguishing from the common used enhanced MOSFET that normally turns ON with applying some voltage to the gate (i.g, VGS > VGS (th) for N-channel MOSFET), a depletion mode MOSFET normally turns ON without applying any gate voltage, which means the MOSFET can turn on when VGS > 0, VGS = 0, or VGS < 0. Because the depletion MOSFET is based on the enhanced MOSFET with positive ions being injected into the insulation layer of the FET. So there naturally exists a conductive channel.

For depleted N-channel MOSFET, the original positive ion field can only be offset once VGS (negative value) is negatively increased further to reach the pinch-off mode at VGS (OFF), or is called VGS (th). Then the conductive channel can be closed.

Figure 3-3 shows the modes of operation with adding the depletion MOSFET Qd to the existing ideal diode controller circuit.

When VCATHODE <= VANODE, the normal operation that VIN >= VOUT. At this time, the bypass circuit of the solar power optimizer works. MOSFETs Q1 and Qd are turned ON, VCATHODE ≌ VANODE.

VCATHODE > VANODE during reverse polarity or reverse current protection operation that VIN < VOUT. At this time, the bypass circuit of the solar power optimizer does not operate. MOSFET Q1 is turned off, MOSFET Qd is in regulation mode as a source follower, maintaining VCATHODE above VANODE, VCATHODE = VIN(VANODE)+ Abs (VGS (th)). So, voltage across VCATHODE to VANODE is within absolute maximum rating VGS (th) of Qd (< 5V. typ) which is far less than the maximum reverse voltage 45VMAX (transient) of LM74610-Q1. Now, the high reverse voltage (VOUT – VIN) is sustained by the drain-source voltage VDS of Qd.

How to choose the right depletion MOSFET mainly depends on two factors.

  • Choose a VDS rating of Qd ≥ VIN(max) (maximum peak input voltage).
  • RDS(on) can be in the hundreds of ohms range (LM746x0-Q1 is floating gate drive architecture with large impedance of CATHODE pin to ground, ICATHODE of the controller is in µA range).
 Modes of Operation With Adding Depletion
                        MOSFET (VCATHODE ≤ VANODE)Figure 3-3 Modes of Operation With Adding Depletion MOSFET (VCATHODE ≤ VANODE)
 Modes of Operation With Adding Depletion
                        MOSFET (VCATHODE > VANODE)Figure 3-4 Modes of Operation With Adding Depletion MOSFET (VCATHODE > VANODE)

Figure 3-5 and Figure 3-6 shows the simulation circuit and results of the bypass circuit with LM74610-Q1 and depletion MOSFET. From the simulation results, this can be seen that using depletion MOSFET is an effective method to extent the reverse voltage range of the current low voltage ideal diode controller, which solves the challenge of very large input voltage range of PV panel or string.

With this design, there also have system benefits to the solar power optimizer system as the following.

  • Solve hot-spot issue due to very low power loss.
  • Make solar equipment be safer, reduce the fire risk.
  • Improve solar power generation efficiency.
 Simulation Circuit of the Bypass Circuit With
                    LM74610-Q1 and Depletion MOSFETFigure 3-5 Simulation Circuit of the Bypass Circuit With LM74610-Q1 and Depletion MOSFET
 Simulation Results of the Bypass Circuit With
                    LM74610-Q1 and Depletion MOSFETFigure 3-6 Simulation Results of the Bypass Circuit With LM74610-Q1 and Depletion MOSFET
Note:
  • Bypass circuit operational, VIN ≥ VOUT
  • Bypass circuit non-operational, VIN < VOUT
  • Simulates input voltage variations
  • Simulates high-transient voltage appears on VOUT , generated by VOV_SIM source
  • Qd operates as source follower, maintaining VCATHODE–VANODE = |VGS(th)| ≅ 1.6V